This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00334-Q1: LMK00334RTVRQ1 PCIe 2.0 Jitter

Part Number: LMK00334-Q1
Other Parts Discussed in Thread: LMK00338,

I plan to use the LMK00334RTVRQ1 as a clock mux/buffer for PCIe 2.0.  The datasheet lists PCIe 3.0 and 4.0 jitter performance, but it does not list 2.0 jitter specs.  What is the 2.0 additive jitter max for the high and low frequency bands with an HCSL clock input and across temperature?  Thanks.

I see a blog post lists typical 2.0 jitter for the LMK00338, but I am looking for max jitter for LMK00334-Q1.