Other Parts Discussed in Thread: CD4020B,
Tool/software: WEBENCH® Design Tools
Dear,
I built the board (PCBA) as the picture below to control the LED blinking at 0.62Hz
The output frequency measured on PCBA is 0.565Hz when starting Oscillating, and the frequency goes up to 0.574Hz after working 10minutes and continues goes up to 0.585 after working 30minutes( measured on 3 PCBAs).
Is the capacitor (C8) heating up and make the capacitance goes down, so the frequency goes up according?
Is the precision of output impacted by the tolerance of C8, R9, R11 mainly or have or other things? are there have any ways to improve the precision of frequency output?
And how about if I use a big resistance for R9 and R11? is the frequency will be an easy impact by the noise of the environment? (since I'd like to use a small capacitor (C8), It help to get the capacitor with 5%tolerace).
Thanks,
Phuoc