Other Parts Discussed in Thread: TMUX6119,
Ronald Michallick very kindly provided analysis and the following information regarding a part of my circuit involving a LM555 timer provided a high and low frequency pulse to a TMUX6119 switch.
As my pervious circuit was so badly wrong, would someone be so kind as to check that this circuit appended below, is correctly configured please?
Thank you so much.
Christopher J James
Christopher,
No interconnects needed. Just connect pin 3 to the select pin on the analogue switch IC. Ground goes to ground. VCC+ can use same positive supply that the analogue switch uses.
The data sheet suggests adding bypass capacitance to power pin (+15V)
0.1 uF bypass ceramic capacitor
1 uF electrolytic bypass capacitor
Using equations in the data sheet , here are the results.
The TMUX needs a VIL less than 0.8V , the LM555 can meet that need.
The TMUX needs a VIH greater than 2V, the LM555 can meet that need.
I have said this multiples times, but I will say it again. LM555 pin 3 can connect to the TMUX directly without any other components.
LM555 low output will be near 0V. This level is valid (less than 0.8V). LM555 high output will be roughly 14V. This level is valid (greater than 2V, but less than or equal to VCC, 15V).
Regards,
Ronald Michallick