Other Parts Discussed in Thread: CODELOADER
Dear Technical Support Team,
Output clock may not be output from LMK03328 after power on.
125MHz and 266MHz are not output. (Using PLL1 and PLL2)
100MHz can be output. (100MHz external oscillator without using PLL)
When clock generator is cooled with the cooling spray while the clock is not output, then clock is output. After that, the clock is output stably.
If you have any information, please let me know.
Attached codeloader file(mac) below.
I can't attach the mac file, so could you change the file name from LMK03328mac.pdf to LMK03328.mac?
Attached schematic and wave of power on below(pdf).
Best Regards,
ttd