Hi, CDCM9102 supprot team,
I understood that the TYPE of OE / OS1 / OS0 pin in the following Pin Functions table is a typo so that it is explained in other thread. And also, not only 25MHz X-tal clock but also AC-coupled 2.5V LVCMOS and DC-coulpled 3.3V LVCMOS signal applied to the XIN.
By the way, which of the assigned pins is the following "LVCMOS INOUTS" erelctrical characteristics specified? Is it only for XIN pin?
If OE pin is LVCMOS input, is 150kohm pull-uped resstor presence?
Thanks
Tamio