This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2581: LMX2581, 0_delay_mode, 2nd Order Modulator.

Part Number: LMX2581


Hi.

I have been using the LMX2581 for a while and now i need to use the 0 delay mode, for phase alignment between the input and output

It works fine for "integer mode", but i wold like to use it for "FRAC_ORDER = 2nd Order Modulator".

I can not get the signals to align properly.

My preferred numbers is 50Mhz inn, 868Mhz out, but i have tried all kind of numbers.

So my question is: Is this even possible to do with this chip?. If not do you have a chip that will do this.

Best regards

Richard