Part Number: LMC555
Other Parts Discussed in Thread: TLC555
Hi, I'm using LMS555 in astable mode. There are three questions confusing me:
1, In the datasheet, Figure 7 astable waveforms, according to the given resistors and capacitors, the output frequency should be 6.58 kHz, namely 152 us per period. But from the Figure 7, each period takes around 68 us, so is the figure here wrong, or I missed something by calculating.
2, I use Ra = 10K ohm, Rb = 100K ohm, C = 10 pF, hoping to get an 685.7kHz output, but indeed I get an output of around 324.5 kHz, So where is the problem?
3, When I remove the C, put nothing between thres pin and ground, there is still an output of around 707 kHz, so is there still a charging and discharging object even I remove the C?
Interesting is that, if we calculate this "virtual" charging/discharging object, it seems the value is around 9.7 pF, this seems an "answer" to the question 2, when the true capacitor(10pf) and this "virtual" capacitor(9.7 pf) are combined. Is there something to do with the stray capacitance? (which I think usually at level of fF on a PCB board).
Can someone give me some clue?
BR,
Bian