This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: Triggered Ramp with no Tone at end (or beginning)

Part Number: LMX2594


We are interested in creating a ramp signal (~40MHz) using the lmx2594.  We have the chip generating ramps (trigger is positive edge on ramp_clk).  What we want is to trigger a set (maybe 10) of ramps, then have a ~100ms time before the next set.  When we do this the lmx is outputting a cw tone at the frequency at the end of the ramp.  We also see this if the "burst" of triggers are spread out, there will be a ramped signal with a solid CW connecting to the next start.

Is there a way to setup the ramp so that the output is muted after ramp_len expires?