Part Number: LMX2594
Other Parts Discussed in Thread: LMX2820
Hi,
We are planning to use your LMX2594 PLL for our wideband freq range of 9000 to 14500MHz.
Our Phase noise requirement at 10KHz offset is -102dBc/Hz. Whereas in you datasheet page No: 14 (Figure 3. Closed-Loop Phase Noise at 15 GHz ) has phase noise -104.8 dBc/Hz at 10KHz offset.
The above phase noise measurement is done Fosc = 100 MHz & Fpd = 200 MHz.
But in our system 10MHz clock will be coming from external for PLL reference. If we use 10MHz clock with phase noise of -175 dBc/Hz at 10KHz offset, The therorical output phase noise at 14.5GHz will be
-175+ 20*log(14500/10) which is around -111 dBc/Hz. But PLL may degrade this level by some amount (Not sure about levels).
1. Is there any huge degradation will be expected if we use 10MHz OCXO O/P to you PLL directly?
2. The Phase noise plots in you datasheets are measured with which 100MHz Reference clock? Can you provide the reference CLK phase noise levels which is used for datasheet measurements?
3. Should we need to use multipliers before PLL ref input to multiply our 10MHz to around 100MHz to meet our requirement of -102dBc/Hz at 10KHz offset?
Our PLL settling time requirement is 100uS (Including PLL write) for your info to consider our loop bandwidth requirements.
Regards,
Sugumar K