Part Number: LMK04828
Other Parts Discussed in Thread: , LMK04808
I use the Dynamic Digital Delay to shift the DCLKs.
I followed the example in datasheet SNA605AS p. 44 and programmed the DCLKoutX_DDLY_CNTH/_CNTL (0x101) according to table 3 and it works to delay the clock.
My Clock Divider is 4, so the CNTH/CNTL is 2/3.
My questions:
1. The datasheet of LMK04828-EP (SNAS703) requires also to program DCLKoutX_DDLYd_CNTH/_CNTL(0x102). Is this also necessary for the LMK04828 (without EP) ?
2. The Table 3 in SNAS605AS describes CNTH/CNTL register settings only for DELAYING the clock. But what are the values when I want to shift the clock in advance?
In section 9.3.3.2 its just written: "by programming a small alternate divider value ..... " But A CNTH/CNTL of 1/2 is not allowed.
Thanks for your support,
Jonas