Part Number: LMX2581
Other Parts Discussed in Thread: LMX2592, LMX2594, LMX2572
Please give advice on how to use PLLatinum Sim.
Isn't the Achieved value displayed in the Parameter of Filter Designer the value of "Total Phase Noise" of Phase Noise?
If not, what is the value of Achieved?
The value of "Total Phase Noise" seems to match the value on the graph.
If I want to optimize the phase noise of MKR1 to -100dBc/Hz or less, should I enter "-100" in "MAX Value"?
Then click Calculate Loop Filter. What does the Achieved value "-92" mean?
Currently, I cannot satisfy -100dBc/Hz.
It may be difficult in practice, but is there a way to set the optimization so that it is closer to that?
If you optimize with the photo settings, you will get characteristics you do not want at all.
The PLLatinum Sim setup data are manually adjusted loop filter constants.
(Is it better to make the final adjustment manually after the automatic adjustment?)
Regards,
Akihiko Yokouchi/