Part Number: LMC555
Other Parts Discussed in Thread: TLC555
Hi Ron-san,
My customer is considering to use LMC555 for the 50% duty cycle oscillator by referring to your below thread.
- [FAQ] How do I design a-stable timer, oscillator, circuits using LMC555, TLC555, LM555, NA555, NE555, SA555, or SE555?
Since they want to calculate the tolerance of the 50% duty cycle, they want to know min/typ/max specification of the following parameters of the LMC555CMX/NOPB.
- Output driver:
- ROH: Min= , Typ=, Max=
- ROL: Min= , TYp= , Max=
- Output delay:
- The output low to high time delay: tPLH: Min= , Typ= , Max=
- The output high to low time delay: tPHL: Min=, Typ=, Max=
Thank you.
Best Regards,
Koshi Ninomiya