This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK5B12204: Need help configuring one output to generate 38.4 MHz clock

Part Number: LMK5B12204
Other Parts Discussed in Thread: LMK05318B, USB2ANY

Hello,
We have a design using the LMK5B12204 that uses Input XO of 19.2 MHz in the CMOS (SE no term) configuration. We would like to generate an output CMOS +/- clock of 38.4 MHz that is synchronized on a 1 pps signal. Could you please provide us with the register settings for this configuration ? We have tried using the TICS Pro wizard in generating the register values but with no success so far. When programming the register values we follow the steps:
1. Pull PDN pin high.
2. Program values of the registers in low to high order
3. Write 1b to the RESET_SW bit in register 0x0C
4. Write 0b to the RESET_SW bit in register 0x0C

When programming the registers we mask the appropriate registers R12, R157,R164 and R353 to R435

We are using SPI at 5 MHz to communicate with the chip. After we write the registers and we read them back the values are not set correctly. Also we can't see any output on the oscilloscope.


Any help will be greatly appreciated.
Thank You

  • Hi Stefan,

    Did you get a chance to read the last page of the wizard and read back status register values? That'll give you a clue of what's not working. I'd manually enable the BAW lock detect first just for evaluation purposes and see if the BAW VCO can lock. 

    If there's some setting that you don't understand, click "show instructions" and read the notes there.

    Regards,

    Hao

  • Hello Hao,

    Thanks for the suggestion.

    I've enabled BAW lock detect with the default settings from the wizard.

    Regarding the last page of the wizard, I've read the Registers ( that I could find, for example PLL2_VM_INSIDE and PLL1_VM_INSIDE are nowhere to be found in the register programming manual).

    LOS_FDET_XO bit is 0, while LOL_PLL2 and LOS_XO bits are 1.  Value of 0x0D register is 0x09.

    LOPL_DPLL, LOFL_DPLL and HLDOVR bits are 1 and  LOR_MISSCLK, LOR_FREQ and LOR_AMP bits are 0.  The value of 0x0E register is 0x0D. I don't know if these values are relevant since DPLL is disabled (as per recommandation of wizard when enabling BAW lock detect).

    BAW_LOCK bit si 0. Value of 0x50 register is 0x00.

    I could not find PLL1_VM_INSIDE and PLL2_VM_INSIDE bits in any registers.

    Could you please guide me in what should I do next ?

    Thank you for your help.

    Regards,

    Stefan 

  • Hi Stefan,

    Actually, you don't need a register manual and you can find all the information in Ticspro. Go to the status page and find all the status registers. Click "read status" button to read back status registers. By the way, the register information can be found in the lower left pane when you hover the mouse over a field register.

    If DPLL is disabled then it'll be a lot easier. The final goal is to get the BAW locked. First make sure that LOS_FDET_XO is cleared which means that XO is valid. If there's still a problem, can you upload your configuration so that I can have a quick look?

    Regards,
    Hao

  • Hello Hao,

    Thank you for your response.

    I cannot read the status from the TICS Pro software as I do not have any connection with it. (Is there any evaluation board of the LMK5B12204 that can be connected to this software ? ).

    We are only using the TICS Pro software to configure the outputs that we want and then export the Hex file with the register values.

    After that we have a microcontroller connected through SPI to the LMK5b12204 and that's the way we program the values of the registers.

    I have attached the register values that we export from the TiCS Pro software. Can you tell us if there's something wrong with these register values ?

    Thank you.

    Stefan

    R0	0x000010
    R1	0x00010B
    R2	0x000235
    R3	0x000332
    R4	0x000404
    R5	0x00050E
    R6	0x000617
    R7	0x00078E
    R8	0x000802
    R10	0x000AC8
    R11	0x000B00
    R12	0x000C1B
    R13	0x000D08
    R14	0x000E00
    R15	0x000F00
    R16	0x001000
    R17	0x00111D
    R18	0x0012FF
    R19	0x001308
    R20	0x001420
    R21	0x001501
    R22	0x001600
    R23	0x001755
    R24	0x001855
    R25	0x001900
    R26	0x001A00
    R27	0x001B00
    R28	0x001C01
    R29	0x001D13
    R30	0x001E40
    R32	0x002044
    R35	0x002300
    R36	0x002403
    R37	0x002500
    R38	0x002600
    R39	0x002703
    R40	0x002803
    R41	0x002900
    R42	0x002A11
    R43	0x002BC2
    R44	0x002C00
    R45	0x002D03
    R46	0x002E11
    R47	0x002F87
    R48	0x003050
    R49	0x00314A
    R50	0x003237
    R51	0x003380
    R52	0x003400
    R53	0x00352F
    R54	0x003600
    R55	0x003700
    R56	0x00380F
    R57	0x003900
    R58	0x003A0F
    R59	0x003BBE
    R60	0x003C2F
    R61	0x003D00
    R62	0x003E63
    R63	0x003F00
    R64	0x004000
    R65	0x004100
    R66	0x004200
    R67	0x004318
    R68	0x004408
    R69	0x004500
    R70	0x004600
    R71	0x004700
    R72	0x004833
    R73	0x004900
    R74	0x004A01
    R75	0x004B00
    R76	0x004C00
    R77	0x004D0F
    R78	0x004E00
    R79	0x004F11
    R80	0x005080
    R81	0x00510A
    R82	0x005200
    R83	0x00530B
    R84	0x005440
    R85	0x005500
    R86	0x005600
    R87	0x00571E
    R88	0x005884
    R89	0x005980
    R90	0x005A00
    R91	0x005B14
    R92	0x005C00
    R93	0x005D0B
    R94	0x005E40
    R95	0x005F00
    R96	0x006000
    R97	0x00611E
    R98	0x006284
    R99	0x006380
    R100	0x006428
    R101	0x006501
    R102	0x006622
    R103	0x00670F
    R104	0x00681F
    R105	0x006905
    R106	0x006A00
    R107	0x006B64
    R108	0x006C00
    R109	0x006D41
    R110	0x006E1A
    R111	0x006FAA
    R112	0x0070AA
    R113	0x0071AA
    R114	0x0072AB
    R115	0x007303
    R116	0x007400
    R117	0x007500
    R118	0x007600
    R119	0x007700
    R120	0x007800
    R121	0x007900
    R122	0x007A00
    R123	0x007B28
    R124	0x007C00
    R125	0x007D11
    R126	0x007E79
    R127	0x007F7A
    R128	0x008000
    R129	0x008101
    R130	0x008200
    R131	0x008301
    R132	0x008401
    R133	0x008577
    R134	0x008600
    R135	0x008790
    R136	0x008800
    R137	0x008900
    R138	0x008A00
    R139	0x008B03
    R140	0x008C02
    R141	0x008D00
    R142	0x008E01
    R143	0x008F01
    R144	0x009077
    R145	0x009101
    R146	0x009289
    R147	0x009320
    R149	0x00950D
    R150	0x009600
    R151	0x009701
    R152	0x00980D
    R153	0x009929
    R154	0x009A24
    R155	0x009B32
    R156	0x009C01
    R157	0x009D00
    R158	0x009E00
    R159	0x009F00
    R160	0x00A0FC
    R161	0x00A132
    R162	0x00A200
    R164	0x00A400
    R165	0x00A500
    R167	0x00A701
    R178	0x00B200
    R180	0x00B400
    R181	0x00B500
    R182	0x00B600
    R183	0x00B700
    R184	0x00B800
    R185	0x00B904
    R186	0x00BA08
    R187	0x00BB00
    R188	0x00BC00
    R189	0x00BD00
    R190	0x00BE2C
    R191	0x00BF00
    R192	0x00C050
    R193	0x00C100
    R194	0x00C200
    R195	0x00C300
    R196	0x00C400
    R197	0x00C51D
    R198	0x00C600
    R199	0x00C700
    R200	0x00C81D
    R201	0x00C900
    R202	0x00CA00
    R203	0x00CB00
    R204	0x00CC15
    R205	0x00CD00
    R206	0x00CE00
    R207	0x00CF15
    R208	0x00D000
    R209	0x00D114
    R210	0x00D200
    R211	0x00D316
    R212	0x00D400
    R213	0x00D514
    R214	0x00D600
    R215	0x00D716
    R216	0x00D80F
    R217	0x00D900
    R218	0x00DA00
    R219	0x00DB19
    R220	0x00DC6E
    R221	0x00DD00
    R222	0x00DE03
    R223	0x00DF0D
    R224	0x00E047
    R225	0x00E100
    R226	0x00E200
    R227	0x00E319
    R228	0x00E46E
    R229	0x00E500
    R230	0x00E603
    R231	0x00E70D
    R232	0x00E847
    R233	0x00E90A
    R234	0x00EA0A
    R235	0x00EB00
    R236	0x00ECC3
    R237	0x00ED50
    R238	0x00EE00
    R239	0x00EF00
    R240	0x00F0C3
    R241	0x00F150
    R242	0x00F200
    R243	0x00F300
    R244	0x00F400
    R249	0x00F912
    R250	0x00FA00
    R251	0x00FB13
    R252	0x00FC24
    R253	0x00FD00
    R254	0x00FE00
    R255	0x00FF00
    R256	0x010000
    R257	0x010101
    R258	0x010200
    R259	0x010301
    R260	0x010402
    R261	0x010580
    R262	0x010600
    R263	0x010700
    R264	0x010800
    R265	0x010900
    R266	0x010AC8
    R267	0x010BA0
    R268	0x010C0C
    R269	0x010D0A
    R270	0x010E02
    R271	0x010F14
    R272	0x011000
    R273	0x011100
    R274	0x011200
    R275	0x01130E
    R276	0x01140C
    R277	0x01150E
    R278	0x011609
    R279	0x011708
    R280	0x011809
    R281	0x011907
    R282	0x011A0D
    R283	0x011B07
    R284	0x011C1E
    R285	0x011D1E
    R286	0x011E02
    R287	0x011F30
    R288	0x012000
    R289	0x0121EE
    R290	0x012202
    R291	0x0123CA
    R292	0x012409
    R293	0x012501
    R294	0x012600
    R295	0x01272C
    R296	0x012808
    R297	0x01290C
    R298	0x012A08
    R299	0x012B01
    R300	0x012C00
    R301	0x012D1C
    R302	0x012E20
    R303	0x012F01
    R304	0x013001
    R305	0x013100
    R306	0x013200
    R307	0x013300
    R308	0x013410
    R309	0x0135AA
    R310	0x0136AA
    R311	0x0137AA
    R312	0x0138AA
    R313	0x0139AA
    R314	0x013AFF
    R315	0x013BFF
    R316	0x013CFF
    R317	0x013DFF
    R318	0x013EFF
    R319	0x013F03
    R320	0x014000
    R321	0x01410A
    R322	0x014200
    R323	0x014324
    R324	0x01449F
    R325	0x014500
    R326	0x014600
    R327	0x014798
    R328	0x014896
    R329	0x014980
    R330	0x014A00
    R331	0x014B64
    R332	0x014C00
    R333	0x014D00
    R334	0x014E27
    R335	0x014F10
    R336	0x015000
    R337	0x015198
    R338	0x015296
    R339	0x015300
    R340	0x015400
    R341	0x015500
    R342	0x015600
    R343	0x015700
    R344	0x015800
    R345	0x015900
    R346	0x015A02
    R347	0x015B00
    R348	0x015C00
    R349	0x015D00
    R350	0x015E00
    R351	0x015F00
    R352	0x016000
    R357	0x016528
    R367	0x016F00
    R411	0x019B0C
    

    R0	0x000010
    R1	0x00010B
    R2	0x000235
    R3	0x000332
    R4	0x000404
    R5	0x00050E
    R6	0x000617
    R7	0x00078E
    R8	0x000802
    R10	0x000AC8
    R11	0x000B00
    R12	0x000C1B
    R13	0x000D08
    R14	0x000E00
    R15	0x000F00
    R16	0x001000
    R17	0x00111D
    R18	0x0012FF
    R19	0x001308
    R20	0x001420
    R21	0x001501
    R22	0x001600
    R23	0x001755
    R24	0x001855
    R25	0x001900
    R26	0x001A00
    R27	0x001B00
    R28	0x001C01
    R29	0x001D13
    R30	0x001E40
    R32	0x002044
    R35	0x002300
    R36	0x002403
    R37	0x002500
    R38	0x002600
    R39	0x002703
    R40	0x002803
    R41	0x002900
    R42	0x002A11
    R43	0x002BC2
    R44	0x002C00
    R45	0x002D03
    R46	0x002E11
    R47	0x002F87
    R48	0x003050
    R49	0x00314A
    R50	0x003237
    R51	0x003380
    R52	0x003400
    R53	0x00352F
    R54	0x003600
    R55	0x003700
    R56	0x00380F
    R57	0x003900
    R58	0x003A0F
    R59	0x003BBE
    R60	0x003C2F
    R61	0x003D00
    R62	0x003E63
    R63	0x003F00
    R64	0x004000
    R65	0x004100
    R66	0x004200
    R67	0x004318
    R68	0x004408
    R69	0x004500
    R70	0x004600
    R71	0x004700
    R72	0x004833
    R73	0x004900
    R74	0x004A01
    R75	0x004B00
    R76	0x004C00
    R77	0x004D0F
    R78	0x004E00
    R79	0x004F11
    R80	0x005080
    R81	0x00510A
    R82	0x005200
    R83	0x00530B
    R84	0x005440
    R85	0x005500
    R86	0x005600
    R87	0x00571E
    R88	0x005884
    R89	0x005980
    R90	0x005A00
    R91	0x005B14
    R92	0x005C00
    R93	0x005D0B
    R94	0x005E40
    R95	0x005F00
    R96	0x006000
    R97	0x00611E
    R98	0x006284
    R99	0x006380
    R100	0x006428
    R101	0x006501
    R102	0x006622
    R103	0x00670F
    R104	0x00681F
    R105	0x006905
    R106	0x006A00
    R107	0x006B64
    R108	0x006C00
    R109	0x006D41
    R110	0x006E1A
    R111	0x006FAA
    R112	0x0070AA
    R113	0x0071AA
    R114	0x0072AB
    R115	0x007303
    R116	0x007400
    R117	0x007500
    R118	0x007600
    R119	0x007700
    R120	0x007800
    R121	0x007900
    R122	0x007A00
    R123	0x007B28
    R124	0x007C00
    R125	0x007D11
    R126	0x007E79
    R127	0x007F7A
    R128	0x008000
    R129	0x008101
    R130	0x008200
    R131	0x008301
    R132	0x008401
    R133	0x008577
    R134	0x008600
    R135	0x008790
    R136	0x008800
    R137	0x008900
    R138	0x008A00
    R139	0x008B03
    R140	0x008C02
    R141	0x008D00
    R142	0x008E01
    R143	0x008F01
    R144	0x009077
    R145	0x009101
    R146	0x009289
    R147	0x009320
    R149	0x00950D
    R150	0x009600
    R151	0x009701
    R152	0x00980D
    R153	0x009929
    R154	0x009A24
    R155	0x009B32
    R156	0x009C01
    R157	0x009D00
    R158	0x009E00
    R159	0x009F00
    R160	0x00A0FC
    R161	0x00A132
    R162	0x00A200
    R164	0x00A400
    R165	0x00A500
    R167	0x00A701
    R178	0x00B200
    R180	0x00B400
    R181	0x00B500
    R182	0x00B600
    R183	0x00B700
    R184	0x00B800
    R185	0x00B904
    R186	0x00BA08
    R187	0x00BB00
    R188	0x00BC00
    R189	0x00BD00
    R190	0x00BE2C
    R191	0x00BF00
    R192	0x00C050
    R193	0x00C100
    R194	0x00C200
    R195	0x00C300
    R196	0x00C400
    R197	0x00C51D
    R198	0x00C600
    R199	0x00C700
    R200	0x00C81D
    R201	0x00C900
    R202	0x00CA00
    R203	0x00CB00
    R204	0x00CC15
    R205	0x00CD00
    R206	0x00CE00
    R207	0x00CF15
    R208	0x00D000
    R209	0x00D114
    R210	0x00D200
    R211	0x00D316
    R212	0x00D400
    R213	0x00D514
    R214	0x00D600
    R215	0x00D716
    R216	0x00D80F
    R217	0x00D900
    R218	0x00DA00
    R219	0x00DB19
    R220	0x00DC6E
    R221	0x00DD00
    R222	0x00DE03
    R223	0x00DF0D
    R224	0x00E047
    R225	0x00E100
    R226	0x00E200
    R227	0x00E319
    R228	0x00E46E
    R229	0x00E500
    R230	0x00E603
    R231	0x00E70D
    R232	0x00E847
    R233	0x00E90A
    R234	0x00EA0A
    R235	0x00EB00
    R236	0x00ECC3
    R237	0x00ED50
    R238	0x00EE00
    R239	0x00EF00
    R240	0x00F0C3
    R241	0x00F150
    R242	0x00F200
    R243	0x00F300
    R244	0x00F400
    R249	0x00F912
    R250	0x00FA00
    R251	0x00FB13
    R252	0x00FC24
    R253	0x00FD00
    R254	0x00FE00
    R255	0x00FF00
    R256	0x010000
    R257	0x010101
    R258	0x010200
    R259	0x010301
    R260	0x010402
    R261	0x010580
    R262	0x010600
    R263	0x010700
    R264	0x010800
    R265	0x010900
    R266	0x010AC8
    R267	0x010BA0
    R268	0x010C0C
    R269	0x010D0A
    R270	0x010E02
    R271	0x010F14
    R272	0x011000
    R273	0x011100
    R274	0x011200
    R275	0x01130E
    R276	0x01140C
    R277	0x01150E
    R278	0x011609
    R279	0x011708
    R280	0x011809
    R281	0x011907
    R282	0x011A0D
    R283	0x011B07
    R284	0x011C1E
    R285	0x011D1E
    R286	0x011E02
    R287	0x011F30
    R288	0x012000
    R289	0x0121EE
    R290	0x012202
    R291	0x0123CA
    R292	0x012409
    R293	0x012501
    R294	0x012600
    R295	0x01272C
    R296	0x012808
    R297	0x01290C
    R298	0x012A08
    R299	0x012B01
    R300	0x012C00
    R301	0x012D1C
    R302	0x012E20
    R303	0x012F01
    R304	0x013001
    R305	0x013100
    R306	0x013200
    R307	0x013300
    R308	0x013410
    R309	0x0135AA
    R310	0x0136AA
    R311	0x0137AA
    R312	0x0138AA
    R313	0x0139AA
    R314	0x013AFF
    R315	0x013BFF
    R316	0x013CFF
    R317	0x013DFF
    R318	0x013EFF
    R319	0x013F03
    R320	0x014000
    R321	0x01410A
    R322	0x014200
    R323	0x014324
    R324	0x01449F
    R325	0x014500
    R326	0x014600
    R327	0x014798
    R328	0x014896
    R329	0x014980
    R330	0x014A00
    R331	0x014B64
    R332	0x014C00
    R333	0x014D00
    R334	0x014E27
    R335	0x014F10
    R336	0x015000
    R337	0x015198
    R338	0x015296
    R339	0x015300
    R340	0x015400
    R341	0x015500
    R342	0x015600
    R343	0x015700
    R344	0x015800
    R345	0x015900
    R346	0x015A02
    R347	0x015B00
    R348	0x015C00
    R349	0x015D00
    R350	0x015E00
    R351	0x015F00
    R352	0x016000
    R357	0x016528
    R367	0x016F00
    R411	0x019B0C
    

  • Hi Stefan,

    I see. You should be able to use a USB2ANY box and bluewire the SPI/I2C lines in order to use Ticspro for evaluation. There's no dedicated EVM for LMK5B12204 and it can be evaluated on a LMK05318B EVM.

    Can you send me the .tcs file instead (File -> Save)? Registers don't contain all the information, such as selections you made in the wizard. You can zip the .tcs file if unable to upload it.

    Regards,
    Hao

  • Hi Hao,

    Attached is the .tcs file with the configuration we use. For now PRI and SEC references are disabled and all we have configured is an output of 38.4 MHz on OUT2.

    Thank you, 

    StefanBawLock.tcs

  • Hi Stefan,

    Now I see. You're not using APLL1 and that's why the BAW is never locked. Still you should see that LOL_PLL2 is cleared and PLL2_VM_INSIDE = 1 if the PLL2 is locked. 

    Can you try enabling the APLL1 and see if you can get the BAW to lock? To do so, you can use cascaded mode (which will provide better performance anyways):

    If you still can't get any PLL to lock, check the capacitor value on pin 29 and 34.

    Regards,
    Hao

  • Hello Hao,

    Thank you for your response. After using the USB2ANY interface and changing the pin 29 capacitor to 0.47 we managed to get the desired frequency and BAW lock.

    Next step for us would be to sync the clock output on a 1 Hz signal incoming on PRIREF input. The signal is a 1 Hz 50% duty cycle signal.

    Can you please give me some starting point on what the settings should be ?

    The DPLL is enabled and  the APLL2 uses  VCO1.

    We set the priref frequency to 1 Hz, DC, hysteresisi enabled.

    We set validation timer to 3.2768s and enabled the 1PPS phase detector with Cntr:64, 1.64 us Jitter.

    We set the DPLL LBW to 0.01

    BAW Lock disabled and DPLL Frequency Lock Detect Phase Detect and Tuning word History set to default.DPLL.tcs

    Is there any status registers that we can check to see if the settings are correct and the DPLL works ?

    We can see on the oscilloscope that the output clock is not synced with the 1 Hz signal.

    Thank you for your help,

    Stefan

  • Hi Stefan,

    Yes. The first register to check is PRIREF_VALSTAT (or SECREF_VALSTAT, depending on which reference you use) which stands for "primary reference valid state". When this register becomes 1 then it means your 1pps signal has been validated and accepted. Only after that will the DPLL start to try to lock.

    You will need a TCXO/OCXO for high frequency precision and low wander otherwise the DPLL won't be able to follow and the reference validation won't pass. The frequency error between the TCXO and 1pps input shouldn't be more than 1ppm.

    If you're able to get the PRIREF to be valid, check DPLL_LOFL and DPLL_LOFL. If both are 0 then you're good to go. The PRIREF_VALSTAT takes about 9 seconds to become valid. DPLL_LOPL usually takes 150-200s. LOFL is faster than LOPL and I can't remember the exact numbers.

    Regards,
    Hao

  • Hello Hao,

    Thank  you for your response.

    We were unable to validate the PRIREF_VALSTAT with 1 Hz input, because we are using 19.2 MHz XO that has +/- 10 ppm. 

    So we decided to switch the PRIREF input to 1 KHz, and now the PRIREF_VALSTAT bit is set, but the LOPL and LOFL of DPLL bits are never cleared ( even after 20 minutes)

    We changed the validation timer to 102.4 ms and disabled all the detectors.

    Should we have any detector enabled for the 1 KHz input ? 

    Can you tell me what I could do next in order to get the DPLL to lock ?

    I have also attached our schematic in case it will help.

    Thank you for your support,

    Stefan.LMK5B12204-TI.pdf

  • Hi Stefan,

    Make sure that you click this button every time you change something. Otherwise the DPLL settings won't be updated.

    In order to run this script, you need to download the matlab runtime engine, which is for free and the link is in the first wizard page. 

    Regards,
    Hao

  • Hi Hao,

    We click the Run Script every time we do any changes.

    But we have set the DPLL LBW to 100 Hz as it was suggested in the instructions.

    Should we set it to 200 Hz ?

    Thank you,

    Stefan

  • Hi Stefan,

    No 100Hz is good. Can you always check if PRIREF_VALSTAT is read back as 1? If the reference is valid and the DPLL script is run then DPLL should be able to lock with no problem. If the reference is indeed valid and the DPLL is not locked, can you read back all the registers and send me the .tcs file for review?

    Regards,
    Hao