This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE62005: Problem using PLLatinum SIM to calculate phase noise performance

Part Number: CDCE62005


Hello,

we are using the CDCE62005 and we want to simulate phase noise performance with respect to some parameters.

Since there is no Webbench available any more, how can we calculate the phase noise output performance of the CDCE62005?

I tried PLLatinum SIM, but when selecting a custom device using advanced feature level I get an error!

Is there an older version which can be used? Or could someone correct this error please?

Version: 1.5.6.0

Error when selecting "custom" in Select Device Field:

Informationen über das Aufrufen von JIT-Debuggen
anstelle dieses Dialogfelds finden Sie am Ende dieser Meldung.

************** Ausnahmetext **************
System.ArgumentOutOfRangeException: InvalidArgument=Value mit dem Wert 0 ist für SelectedIndex ungültig.
Parametername: SelectedIndex
   bei System.Windows.Forms.ComboBox.set_SelectedIndex(Int32 value)
   bei TIPLLatinumSim.TIPLLatinumForm.SelectDeviceComboBox_SelectedIndexChanged(Object sender, EventArgs e)
   bei System.Windows.Forms.ComboBox.OnSelectedIndexChanged(EventArgs e)
   bei System.Windows.Forms.ComboBox.set_SelectedIndex(Int32 value)
   bei TIPLLatinumSim.TIPLLatinumForm.ResultsListBox_SelectedIndexChanged(Object sender, EventArgs e)
   bei System.Windows.Forms.ListBox.OnSelectedIndexChanged(EventArgs e)
   bei System.Windows.Forms.ListBox.WmReflectCommand(Message& m)
   bei System.Windows.Forms.ListBox.WndProc(Message& m)
   bei System.Windows.Forms.Control.ControlNativeWindow.OnMessage(Message& m)
   bei System.Windows.Forms.Control.ControlNativeWindow.WndProc(Message& m)
   bei System.Windows.Forms.NativeWindow.Callback(IntPtr hWnd, Int32 msg, IntPtr wparam, IntPtr lparam)

Best regards

Marco