This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC555: Abnormal Operating Problem

Part Number: TLC555


Hello

I designed the circuit with TLC555 as below image.

I had a problem with output without TRG signal during testing.

Green (U17-3Pin), Purple(U17-2Pin)

What is the cause of the output when there is no TRG signal?

Best regards.

  • Hi Louis,

    Can you probe the supply line when the extra output pulse occurs. It may be helpful to add an additional 1uF bypass capacitor to your supply.

  • Hi Katlynne

    I'm Sorry for the late feedback.

    .I changed it to 1uF bypass capacitor, but the symptoms are the same.

    I attached a waveform image of the power supply

    Do you have any history of case these problems?

    Should I change the TLC555?

    Best regards

  • Hi Louis,

    Just for clarification, was there an incorrect output during the waveform of the power supply you attached in the last image? I'd like to see what the VCC at the TLC555 looks like at the same time an incorrect output occurs. The TLC555 recommends a 0.1uF and a 1uF capacitor on the supply placed near the timer. This is a problem we see occasionally and it's usually attributed to power supply noise.