This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04803: LMK04803B -TICS PRO-PLL2 is not locking

Part Number: LMK04803


Hello, 

We are using LMK04803B on our board and the output measured frequencies are not at the expected values. TICS PRO has been used for the settings and the output has been programmed for 10MHz and 25MHz but we are getting 10.9 MHz and 27.24 MHz; around 9% increase in the frequencies. Please see the attached figures and I will be thankful if you could provide some feedback.

Sincerely,

Nasim.