I am utilizing LMX2594 in full assist mode, only fixed set or frequencies is used, thus look-up table was created first with calibration values.
- I want to ask regarding the valid range of DACISET especially for VCO7. I read-back the value 217 at room temperature and f=14.99GHz, but the valid range is 323...244. Is it OK? Or shall I respect the range in the datasheet and load the value 244? I calibrated it with ACAL_CMP_DELAY 10 and 32.
- In the full-assist I set bit FCAL=0, the Lock Detect works OK. But there is a E2E-post from 22 Oct 2018, where FCAL=1 is recommended in the full assist mode. May I expect strange behavior for FCAL=0 even in the full assist mode?