Tool/software:
Hello team,
My customer is using PCA8565 for clock, may you recommend an automotive alternative? I2C is required.
Thanks.
Regards
Daniel Wang
Tool/software:
Hello team,
My customer is using PCA8565 for clock, may you recommend an automotive alternative? I2C is required.
Thanks.
Regards
Daniel Wang
Tool/software:
Hello team,
My customer is interested in using BQ32000 for their oven project.
If you have any test reports on back-up power charge time based on 0.22F & 0.33F supercap, or any related materials, could you please share…
Tool/software:
Dear TI Support Team,
I hope this message finds you well.
I am currently evaluating the RTC BQ32000 models paired with a 32.768kHz crystal and would like to understand the expected daily time drift when using these…
Tool/software:
Hi Team,
Customers reported that the value of the Years register read from the initial device is 0x6f, which is different from the default value in the datasheet. And I see that the default value is 0xxx. I want to…
Tool/software:
Hi team,
Does it OK to leave BQ32000 VBACK pin floating?
Thanks and Best regards,
Will
Tool/software:
Hi
Our product uses this RTC IC, and it has already been implemented in a large volume of mass-produced products.
Currently, we are encountering an issue with a new model, but the RTC circuitry, layout routing, test…
Tool/software:
Hi
I am using B0510-2R5224-R (Supercapacitors / Ultracapacitors .22F 2.5V EDLC B SERIES CYL) supercapacitor for backup.
Is this will work or suggest me a supercapacitor to use with BQ32000.
THANK YOU.
Tool/software:
Hi Team
I would like to ask you to confirm whether Pin7_IRQ of BQ32000 can output a 32.768kHz square wave?
Thanks,
Boyan
Tool/software:
Tool/software:
Hi Team,
BQ32000 is 1.75mm height, but customer request <1mm height.
Do we have thinner package solution for RTC?
Thanks.
Regards,
Terry
Tool/software:
Hi,
We are using a custom board based on am62x SK and using BQ32000 RTC with Super Capacitor as Backup.
After updating linux system time with date command and updating RTC with hwclock command. After couple of hours…
Tool/software:
Hi guys,
I gone through BQ32000 Datasheet and didn't find any register related to Battery Low warning feature,
Can you Please confirm the same.
Thanks
Shivaji Y
Hi, Support Team
do we have different temperature about timer accuracy ppm? (-40 to 85 deg), (85 to 105 deg),(105 to 125 deg)
if any suggestion, Please advise me.
Thanks,
Best regards…
Hello expert,
customer has one question as below. They are afraid of leakage current from VBACK to VCC and BU has already confirmed there should not have leakage current. But they would like to know why we have two paths(with diode…
Hi, Support Team
We would calculator BQ32000DR about Power Dissipation.
PD=(Tj-Ta)/ ThetaJA=(150°-25°)/114.8=1.08W
is correct?
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Hello expert,
May we know if there is leakage current flows through all the switch from Vback to VCC? Customer would like to save power from VBACK and don't want leakage for it.
Best regards,
Ann Lien