Other Parts Discussed in Thread: LMK04033, LMK04826, LMK04821
Hello,
We are in the process of redesigning a couple of our boards and presently use the LMK04033. The problem we are running into is the synchronization function that allows the aligning of the output clock edges is not deterministic for this device and thus prevents us from reliably synchronizing multiple boards to within one clock period of the clock distribution path in a repeatable manner. This is due to the slow internal slew rate of the SYNC that is being sampled at a . We are hoping that the LMK04826 overcomes this issue. Our goal is to be able to consistently sample the SYNC signal using the distribution clock edge in a deterministic manner. Questions follow:
1. If the SYNC input pin doesn't suffer the slow internal slew rate issue than can you provide the setup and hold time required for this signal so we can guarantee we get a deterministic result?
2. Does using CLKin0 as the SYNC input avoid the slow slew rate issue and if so what are the setup and hold times for this mode?
3. Can we use SYSREF in a deterministic manner to align the clock outputs?
4. What is the sampling rate of the SYNC signal for the LMK04828B and do you have a better timing diagram for this process?
Thanks!