Hi,
My device uses ADS1298, and everything runs OK. The data collect is OK. I have used it for several years.
Recently, I find that when the ADS1298 is started by writing the ADS_START (0x08) command, the first data read after start is "0" for all of the 8 channels.
After that, everything runs OK forever.
That only happens at the first frame I got after writing the ADS_START (0x08) command.
Is it common for the ADS1298 chip? Or is it a problem maybe in my program?
Thank you.