Other Parts Discussed in Thread: ADC12DJ5200RFEVM
Hi Team,
Assisting on a customer on an inquiry, hoping for your inputs.
ADC evaluation board ADC12DJ5200RFEVM and TSW14J57EVM. Please see this link for ADC12DJ5200RFEVM:
www.ti.com/.../slau640.pdf
TSW14J57EVM is not registering the REF CLK from the ADC. LED D4 is not lit. I followed the instructions in the manual. It seems a bit more involved. ADC CLK need to set to 260MHz. Check if LED D4 is on. HSDC software that I am using is SLWC107W.ZIP (Rev. W). Instructions says to install the patch but the patch doesn't install perhaps since HSDC software version is already patched?
Boards are setup as per instructions on page 10 of:
www.ti.com/.../slau640.pdf
I do not have a bandpass filter on 5200 MHz sampling clock. ADC software seem to work fine but I cannot uncheck the checked boxes. Seems like something off with the software. Like Cal Triggered/Running doesn't uncheck if I click as per instructions on page 13. So there is no way to tell if steps are followed correctly and ADC is outputing signals.
Thank you.
-Mark