Other Parts Discussed in Thread: CDCE62005
Hi there,
We are using the DAC34sh84 in a custom board designed in house. We use the complex mixer to create a RF signal from I and Q components.
I am experimenting some strange behaviour when trying to send small signal values.
As I said I send I and Q values to the DAB interface, I enabled x4 interpolation, configure the NCO and use the complex mixer to have in IOUTA a signal as RF = I*cos()-Q*sin().
When I send a small value with 0º phase I = 0010h and Q = 0000h I can see in the sprectrum analyzer a power of -57dBm
When I send I = FFFFh and Q = 0010h, that is, the same value but with 90º I can see in the spectrum analyzer that the power of the RF signal is -62dBm.
I can not undertand this difference in power. Indeed in the second case, our system is transmiting FFFFh instead of 0000h, so we should expect some little increase in the power but never a reduction.
We operate in twos complementes so FFFFh must be almost as 0 as 0000h.
I can see this behaviour wven with values higher than this but as the value gets higher this effect is less significant.
Any clue?
Thanks in advanced,
Juan.