Other Parts Discussed in Thread: ADS124S08
Hello,
I have a typical wheatstone bridge application with 4x active strain gage elements. In my case I cannot use voltage excitation, and hence must use IDAC current excitation for the bridge (currently using 500uA). Due to an additional external INA gain stage, I am looking to apply the AC excitation to remove this offset and drift. However, I do not see any reference designs using AC excitation with the internal IDACs - is there anything preventing this?
If not, it would be great to see a diagram similar to Figure 97 in the datasheet, with IDAC excitation.