This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8411: Vcc=4V with 3.3V SPI

Part Number: DAC8411

Hello Team,

Our customer is considering using DAC8411 @ VDD = 4V with a 3.3V SPI.

What is the Serial clock frequency in this case, 20MHz or 50MHz?

I think it is 50MHz on the datasheet, is that correct?

Regards,

Masakazu