Part Number: ADS1262
Dear sir,
Request you to help me with the following queries:
I am Programming the IC from FPGA.
note:
1.RESET/PWDN pin always high, and using internal reference ,continuous conversion, gain 32, mux reg-- AIN0(POSITIVE ),AIN1(NEGATIVE) and not using commands to read the data
Q1. I am programming the IC from FPGA with following steps:
step 1. start(pin)=0.
step 2:writing to power register
step3: writing to interface register
step4: writing to mode0 register
step5:writing to mode1 register
step6:writing to mode2 register
step7:writing to inputmux register
step 8:start(pin)=1 and stopping the sclk.
step 9:waiting for drdy to low, if low go to step10 otherwise in step 9
step 10:read the data 32 bit.......starting the sclk and send 32 sclk cycles to read
step 11:going to 8.
If i am following the above sequence i am able to read 7FFFFFFF only data .output is not changing when i am moving the input voltage(source +/- 2.5 V).Request you to help me with this problem by suggesting the proper sequence for data acquisition.
Q2.
As far as my understanding is concerned it takes 32 clock cycles to read 32 bits of data from this adc via spi, but data sheet speaks about only 16 cycles for data retrieval with respect to this ic(page no 68, figure 108 , point 3).can you elaborate on this a little how to understand this interms of data acquisition.