This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1018: SPI issue (DOUT)

Part Number: ADS1018

Hi team,

Could you please look into an issue for DOUT level of ADS1018?

Problem: 

-. DOUT never goes to low level (0V).

-. The waveform keeps high even when isolating DOUT from MCU. 

Any check point?

CH1:CS / CH2:CLK / CH3:DOUT / CH4:DIN

Thanks,

Sam Lee

  • Sam,

    I suspect that your DOUT line is shorted to something that is forcing it high.  You may want  to double check the soldering connections.  If you are using the VSSOP package can you de-solder DOUT pin, lift it, and measure the pin directly?  Otherwise, can you cut the trace near the pin and measure the pin directly.  

    Best regards,

    Art