Part Number: ADS4229
Hi:
The ADS4229 in LVDS mode sends out data on both clock edge. On the rising edge it send out data from channel 0 and on the falling edge it sends out data from channel 1.
After I register the data from channel 0 on rising edge and from channel 1 on falling edge, I have to present both data together (to be processed together) . How do I start receiving data so that data from channel 0 and 1 are lined up (in sync) ?
For example when in "sync", sample 0 from channel 0 is latched (present together) with channel 1; sample 1 from channel 0 is latched with channel 1; etc. (0,0 ; 1,1; etc.)
When NOT in "sync", sample 0 from channel 0 is latched with sample 1 from channel 1; sample 1 from channel 0 is latched with sample 2 from channel 1; etc. (0,1 ; 1,2; etc.)
Thanks
Hai