Part Number: ADS8634
Hello Community,
unfortunately I have a problem with the SPI communication of the ADS8634.
I try to write some register and read them afterwards, but I always receive the same wrong data.
AL_PD pin is floaten, Clock is 2MHz
Steps I do:
-Sent reset massage (Transmitt: 0b0000001000000001)
-Write to Adress 06h to enable internal tempsensor and internal reference. (Transmitt: 0b0000110000000110)
-Read also adress 06h but get random data on miso line. (Transmitt: 0b0000110100000110)
I am very happy if somebody can help me.
Two Dataframes you can see in the picture:
Thanks a lot.