Part Number: DAC61402EVM
Other Parts Discussed in Thread: DAC61402, DAC81402
Good day. I have a question about the reference on the DAC61402 as part of the BP-DAC61402EVM eval board. I was able to get the software for the BP-DAC61402EVM to communicate with the controller and the Launchpad controller has been successfully updated/verified with the latest firmware per the datasheet instructions. Pins 1-5 on J17 are at the appropriate voltages as well. I tried measuring the DAC's internal reference and got 2.404V. There is no jumper on J16 so the external 2.500V reference is disconnected. Thinking that the DAC might have been damaged from ESD, our re-work person replaced the DAC on the eval board with one of two that we purchased from a popular online vendor (while carefully following ESD precautions this time). The internal reference of the new DAC measured 2.386V. Based on the datasheet for the DAC61402, this is outside the min/max for the 2.500V internal reference. I can disable the internal reference by toggling bit 13 of the GENCONFIG register. However, the datasheet (and software) states that bit 14 is the ref powerdown bit. When we toggle that bit, we get no response from the DAC (the internal ref doesn't change). I have probed the SPI lines from the controller and the clock, SDI, and SYNC all appear to be transmitting the correct data. On top of all this, I still am unable to get a non-zero output on any of the DAC channels when using either the internal reference or the external reference (which is 2.500V). Is there a particular reason that the internal references measure around 2.400V instead of 2.500V? I'm using a Fluke189 with Kelvin leads so I don't believe a drop in the probe leads are giving incorrect readings. Any suggestions as to what the issue might be would be greatly appreciated.
Thanks,
John B