Part Number: ADS1113
Hi Experts,
A customer is having trouble using this part for their design.
If they set the address to 0x48/0X49, the part works well, but if they connect the address to SCL/SDA (0X4A/4B), the part doesn't work.
In the datasheet, there is a note stating: "Use the GND, VDD and SCL addresses first. If SDA is used as the device address, hold the SDA line low for at least 100 ns after the SCL line goes low to make sure the device decodes the address correctly during I2C communication." The customer have 700nSec between SDA and SCL > 100nSec but still, there is no output from ADS1113.
I attached two pictures for reference.


I hope you can help to solve the issue.
Regards,
Marvin