Part Number: ADS7038-Q1
Other Parts Discussed in Thread: TPS745-Q1
Hi Team,
we want to measure in our application the battery voltage of 32V. It is connected with an voltage divider, to that we limit the current at the input pin to max. 0.57mA.
But for sure the voltage will be available (due to power sequencing) before AVDD and DVDD is available. Is this a problem?
With a look on the absolute maximum ratings we would exceed the maximum allowed voltage, since it is dependent on AVDD. Can we destroy the ADC during power up phase in this scenario?

Thank you,
Fabian