This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSC2003: Deisigning with TSC2003IPWRQ1

Part Number: TSC2003

Hello Team,
I am using TSC2003IPWRQ1 in one of our touch displays.
My display is a resistive touch display.
The display has XR, XL, YU, and YD pins for touch data.
Can I connect the X+ pin of the IC TSC2003IPWRQ1 to any of the XL or XR pins of the display?
Similarly for Y direction pins?
Can I interchange the X and Y direction pins of the display with that of the IC?
That is X direction pins of the display  to Y of the IC and Y direction pins of the display to the X pins of the IC

  • Hi Shibin, 

    Since the connections from XR/XL is simply a resistive element it wont have a polarity  there should be no issue to connect X+/X- to either XR/XL.

    the same can be said for connection X+/X- to the y terminals of the screen

    Regards,
    Arthur