This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1148-Q1: supply current requirement especially during startup

Part Number: ADS1148-Q1
Other Parts Discussed in Thread: ADS1148

Hi,

The I_AVDD is 225µA typ for AVDD=5V according to the datasheet. I assume something similar value applies to +/-2.5V analog supply. The chip seems to consume a way more current during startup.

Can you give a maximum specification that covers the startup too?

What about any timing / slew rate / monotonicity constrains for reaching the recommended supply voltage range (+2.25V)?

Thanks,

Tamas

  • Hi Tamas Fenyvesi,

    Do you have a scope shot, etc. to share that shows the current draw you are seeing on powerup? It would be helpful to see this information.

    The current draw in the datasheet is a typical average current. The instantaneous current draw can be higher, especially on powerup and when integrated features are turned on e.g. PGA, reference, IDACs, etc. I do not have any information to share regarding the instantaneous current draw for this device however.

    I am not aware of any specific power supply timing or ramp requirements for the ADS1148-Q1. I would suggest ensuring that the supplies rise monotonically to make sure that the power-on reset (POR) circuit fully releases so the part can operate normally.

    -Bryan

  • Hi,

    if the supply current is limited, then the ADS1148-Q1 supply voltage creates a valley together with the current limit. The valley looks similar to a MOSFET gate voltage.

    If the current limit/budget is e.g. 10mA, then the valley might take something like 5..10ms. If the supply current is more limited, then the time duration of the valley increases. If the time duration is longer than a certain value, then the ADS1148-Q1 fails working.

    Br,

    Tamas

  • Hi Tamas Fenyvesi,

    I am not sure what you mean by "valley" in your previous post. Are you referring to something like a brownout condition where the supply fails to ramp to the final voltage and instead gets stuck at an intermediate voltage for some time? Again, it would be helpful to see this on a scope so we can more clearly understand the issue you are seeing.

    Anecdotally I have seen that other, similar ADCs can require 10mA or more of instantaneous current. It therefore makes some sense that you are having issues when you restrict the supply current limit to <10mA.

    Are you able to increase the supply current limit in your system to accommodate for these short bursts of current?

    -Bryan

  • Hi Bryan,

    yes, exactly as you wrote: the supply voltage gets stuck at a certain voltage for a while rather than reaching the recommended range by a continuous ramp.

    We modified the supply current source for allowing more current. Anyway, given we are talking about more than 20 times higher current than what the datasheet communicates, we need valid specs that covers the scattering and the full temperature range for a correct calculation and sizing.

    Br,

    Tamas

  • Hi Tamas Fenyvesi,

    Typically we see our ADCs being paired with power supplies + low noise LDOs that can regulate 100s of mA of current, even if the ADC does not require this amount of current. Therefore, this isn't a common challenge. I am glad you were able to modify the power supply to increase the current limit. Did this resolve the issues you were having?

    As I stated in my previous post, the 10 mA value is just anecdotal evidence from other devices, it is not meant to be a hard requirement for the ADS1148-Q1. In fact, the ADS1148-Q1 could be quite different, as I am unaware of any test data that identifies the instantaneous current draw for the ADS1148-Q1. I presume you could measure instantaneous current consumption using a high-speed scope if this more detailed information is required for your application.

    -Bryan

  • Hi Bryan,

    (Regarding technical part, an automotive LDO is easy for positive, but much less options are available for the negative. On the other hand, ADS1148 can be used in micropower/wearable environment, e.g. medical (ECG), where the bottleneck is not necessarily the LDO.)

    Whether LDO or something else, also whichever application area, if the current consumption is so much higher than the datasheet value even temporarily, then the datasheet ought to include hints as a very minimum. (Not to mention that the manufacturer ought to exactly know any potential causes of such an effect for avoiding any internal latch-up in my logic.) Any relevant estimation needs deep knowledge of internal structure and technology - which only the manufacturer has.

    It isn't satisfactory to conclude "folks usually don't see such effect - but some do", since it is products with responsibilities.

    So, what's the specification, please?

    Thanks,

    Tamas

  • Hi Tamas Fenyvesi,

    Let me see if I can look into this in more detail. Please note that this may take some time e.g. a week or more, before I am able to get the setup and equipment ready, take data, and summarize the findings

    Also please note that should we provide data on this issue, it is not guaranteed since it is not included in the ADC datasheet. Therefore you use it at your own risk. I just want to level-set expectations so there is no confusion moving forward.

    -Bryan

  • Hi,

    Thanks and looking forward to hearing from you.

    Please also note that we've seen large variance in the inrush current, therefore some kind of analysis seems more usable than experimental verification of one/few pieces.

    Kind regards,

    Tamas

  • Hi Tamas Fenyvesi,

    In the meantime then, can you share your system schematic including the ADC, any signal conditioning circuitry, and the power supply? It would be worth also checking to make sure this is not a different applications issue.

    If you do not want to share this information on a public forum, you can send it to me via private message. Please hover over my user name and then select "Request friendship". This will allow us to share messages privately

    -Bryan

  • Hi Tamas Fenyvesi,

    I just wanted to let you know that we are still looking into this issue, but I have nothing concrete to share with you at the moment.

    In the meantime, would you be willing to share your schematic including the power supply so we can double-check for any applications issues? You can use the process I outlined in my last post if you do not want to share your schematic in a public forum.

    -Bryan

  • Hi,

    Thanks for updating. I'll send the related schematic part soon - I've been just flooded a bit - we all know this situation

    Kind regards,

    Tamas.

  • Thanks, we will continue working on our end, no rush on the schematic.

    -Bryan