Other Parts Discussed in Thread: ADS1298
Respected,
I am working on a project using the ADS1298R, and i was referring the respiration circuit. But to my surprise the reference respiration circuit provided is different in all documents.
Attached is the pics and references.
1. ADS1298 Datasheet (Page No. 89)
In this Resp_Mode_P is connected to LA and IN1P & Resp_Mode_N is connected to RA and IN1N.
2. ADS1298R PDK (Page No. 41)
In this Resp_Mode_P is connected to LA and IN1N & Resp_Mode_N is connected to RA and IN1P.
3. SBAA181 (Page No 8)
In this Resp_Mode_P is connected to RA and IN1P & Resp_Mode_N is connected to LA and IN1N.
Q1. Kindly clarify which one is correct and can be referred for my circuit.
Q2. Also while i am the first channel as ECG Signal V1, then the Resp Mode P/N are not going to disturb the signals. (provided jumpers @ IN1P/IN1N).