This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC3283: phase noise detail of the part-Reg

Part Number: DAC3283

Hi,

      We are planning to use the DAC3283 in our project design, Kindly share the phase noise of the DAC's output. Refer the below details.

Clock input : 800MHz

Output frequency : 300MHz

Note: PLL(if provided internally) to be disabled for DAC sampling clock.

Also share the phase noise of the clock frequency used. It will be very helpful.

Regards,

Deva.