Other Parts Discussed in Thread: ADS1298
Hi,
We need some help regarding the lead off detection function.
We are using the DC Lead off detection mode with 95% - 5% as a COMP_TH.
More than frequently, our device with ADS1294 triggers the lead off function even when the electrode(s) are intact and connected to the human body.
We would like to troubleshoot it but, first of all, we have no idea the COMP_TH.....95% relative to what voltage ??
Thanks,
Shin