Hi,
We use the DAC161S997 for our 4 - 20mA pressure transmitter.
Now we have the problem, that if we use a high load resistor (510R) and a supply voltage of 24V, The DAC goes straight to loop error when we send as first DAC setting a value close to DAC-MAX (0xfff). The only work around we found till now is, to step up tu the DAC_MAX value with 4 to 5 steps. Is our problem known? Have you other possibilities to prevent the DAC from going to error loop? (Not to reduce the load resistor).
Kind regards sarah