I have 2 differential amplifiers giving same output signal. To rout analog inputs without vias i need to connect the input channels as in image. The differential input varies from 1.2 to -1.2V.
Is below one the effect of this connection?
1. if 1.2V output of Diff amp_1 give 0xE000 at ADCchannel A, 1.2V from Diff amp_2 give 0x2000 at ADCchannel B
2. Is there anything else to consider on HW design?