Part Number: ADS5402EVM
Other Parts Discussed in Thread: ADS5402,
Hello, I am trying to get a sinusoidal signal into a PC using an AD converter.
I am trying to get a sinusoidal signal into a PC using an AD converter.
I am using ADS5402 / ADS5402EVM / TSW1405. The frequency of the input signal is 155 MHz, and when the sampling frequency is set to 800 MHz and a capture is performed, only noise appears, and the FFT result also shows only noise.
Is this because the clock signal is not input?
I thought it was operating with an internal clock, but am I wrong?
こんにちは.
私は,AD変換器を用いて正弦波信号をPCに取り込もうとしています.
使用しているデバイスは,ADS5402 / ADS5402EVM / TSW1405 です.入力信号の周波数は155MHzであり,サンプリング周波数を800MHzと設定しキャプチャーを行ったところ,ノイズしか現れずうまく波形を取得できませんでした.FFT結果についても同様にノイズしか確認できませんでした.
この原因は,クロック信号を入力していないからなのでしょうか.
内部クロックで動作していると考えていましたが,間違っていますでしょうか.