Dear Sir
1. Hardware schematic diagram using the ADS8166:
The input is eight 0-4.096V single-ended signals. The ADC is configured in pseudo-difference mode. The internal reference, reference buffer, REFBY2 buffer are enabled. The measured pin voltages of REFP (4.096V) and REFBY2 (2.048V) are correct. The pin voltages of DVDD (+3.3V),AVDD (+5V) and DECAP (2.8-2.9V, with slight differences among different chips) are correct.
The following figure shows the connection between ADC and C280039CSPZ.
At present, normal ADC conversion results cannot be obtained, because DSP software engineers are not familiar with this kind of ADC register configuration and operation. I hope you can help to provide relevant technical support.