This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8598H: Connecting several ADS8598 on same parallel bus

Part Number: ADS8598H

Hi,

I would like to connect 2 ADCs on same parallel bus. In datasheet, one sentence is not clear/strange for us:

"7.4.2.3.1 Parallel Data Read

For applications that use multiple devices in the system, the CS and RD input signals must be driven separately."

So is mean that we need 2 CS and 2 RD lines ?

So the ADC is active if the RD line goes low even if CS is high ?

Before reading this sentence, I was thinking to connect all inputs together expect the CSs.

Do you have a reference schematic for multiple devices ?

Thanks for your help,

CYril Rupf