Part Number: ADS7067
Other Parts Discussed in Thread: ADS7951
Hi,
is there an option to shut down the internal clock of ADS7067 and connect with an external clock only?
thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I wanted to use only an external clock of 32MHz and eliminate other noise that can be caused by the switching of the internal clock.
is there other model from TI that has this option? the sample rate is around 500KSPS.
thank you!
Roee,
I hope this information is helpful to you.
Art
Hi, thank you so much for the elaborated and well explained answer. it sure did help a lot and made to refine some of the requirements for selecting my ADC.
the thing is, that this ADC would be in use just for a short time for each operation of the entire board, so I thought it would be good if the components would have a shut down mode that turns off the internal switching and waiting in stand by mode.
is there such a component that is also capable of sampling in a rate of 300KSPS (14-16 bits)?
thanks you,
I very appreciate your help!
Roee,
The two devices I mentioned (ADS833x and ADS7951) can both run at lower sampling rates. The ADC128S102 is a good option if you are ok with 12 bits. In general, you can expect older generation and lower resolution devices to use the SCLK as a conversion clock. Again, I would suggest that restricting your design to devices in this class is not a good idea. The modern devices with internal clocks are low noise and low emissions. Also, any external clock will have much greater emissions than internal clocks.
Art