This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8519: ADS8519 +/-10V Input setup

Part Number: ADS8519
Other Parts Discussed in Thread: ADS8509

Hello,

I am considering jumping from ADS8509 to ADS8519 ADC. I would like to avoid as many changes as possible to the surrounding circuitry (including the ADS8509 +/-10V input range connections). When computing how the voltage is divided internally given the old ADS8509 external setup, I get close to the same ratio. Do you foresee any issues with this? I am attaching the ADS8509 bipolar 10 input range set up and internal circuitry of ADS8519 for reference.

 *+/- 10V ADS8509 Connections. I would keep all external connections the same but instead use ADS8519.

 *ADS8519 Internal Setup. (I believe the 25.67K resistor should be connected to ground btw)