Hi All,
I want to use ADS1298 for ECG application with following requirements;
- 5 electrodes (7 lead) ECG.
- Pace detection for 0.1ms to 2ms pulse width.
Question regarding ADS1298;
- What is the Max possible sampling rate which can be supported by ADS1298's SPI with Gain of 12 and 4 channel of ECG signals?
- If 32KSPS sampling rate is selected then the digital filter will have LP cutoff at 0.262*fDR Hz = 8.3KHz ?
- Anyway possible to disable this sinc decimation filter?
- 8.3KHz will not be able to detect 0.1ms Pace pulse, so how this will be addressed? Datasheet claims ADS1298 supports systems meeting IEC60601-2-27!!
Best regards,
BM