Our customer designed an ECG product using ADS1298. Now doing product certification, the industry requires passing 6KV ESD testing. During the implementation room testing, it was found that static addition of 6kV to the channel input interface or USB interface can cause data errors. These interfaces are protected by adding ESD devices, and the ESD model used on the circuit board is WS6183KS.
Now we hope to solve this problem through both hardware and software solutions.
1. Are there any more suitable ESD devices recommended for testing in terms of hardware? Is there a better recommendation for the placement of ESD devices? Or do you have better ESD testing experience to share with us?
2. Can the software determine if the data is incorrect? If the program knows that the data is abnormal due to ESD interference, can the software reset ADS1298 and restore it to normal working state? The customer can also accept this method.