This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC08100EVM: ADC08100CIMTCX - Possible to use TMS320 HRPWM as CLK?

Part Number: ADC08100EVM
Other Parts Discussed in Thread: ADC08100

Hello, I'm planning is to use both TMS320F28374DPTPT and ADC08100CIMTCX.

It is my first time using the ADC08100. May I ask some questions.

Q) The ADC08100 datasheet says:

Although the ADC08100 is tested and its performance is ensured with a 100 MHz clock, it typically will function well with clock frequencies from 20 MHz to 125 MHz.

If FCLK = 125MHz, does this mean VIN will be sampled at 125MHz, just like "Figure 1. ADC08100 Timing Diagram"?

I was confused because the datasheet also said: Maximum Sampling Frequency 100 Msps.

The VIN signal will be a signal with 32.1 MHz max frequency.

Q) TMS320F28374DPTPT can use HRPWM where max f_HRPWM is 100MHz.

https://www.ti.com/lit/ds/symlink/tms320f28375d.pdf?HQS=dis-mous-null-mousermode-dsf-pf-null-wwe&ts=1682310566590&ref_url=https%253A%252F%252Fwww.mouser.com%252F

So I think I can create a 100MHz PWM square wave signals from the TMS320.

Can I use this to supply the 100MHz clock to the ADC08100?

Thank you for your help!