Hi Guys,
I have a board designed according the ADS1298 EVM circuit. I got the current of AVDD less than 1mA when add AVDD=3.3V,ASS=0V,DVDD=3.3V first time.
when i add the voltage above again the current of AVDD went to more than 10mA 。I didn't connect RESET pin with high or low. I found the current of AVDD typical value is about 3mA.
I found the reset pin pull high in EVM circuit.Does the reset pin must be high when power on?
Does the reset pin is floated will cause the AVDD current rise to 10mA?
Thanks!