Other Parts Discussed in Thread: ADS1299
Hi,
I got a EVM of ADS1298 for testing. I used a DMM for current test on EVM JP24 between VCC3.3V TP10 to DVDD as pictuer shows below:
I got beyond 200mA (momentary)current and about 80mA(continuous) by DMM .But in the datasheet 7.1 Absolute maximum ratings input current is 100mA (momentary). And in the datasheet 7.3 IDVDD is noly 0.5mA.
Anyway the EVM is still working and i can get the id and data from it.
So i was confused about the current of DVDD that i tested .compare to the datasheet.
By the way ,the AVDD and AVSS current is about 1.79mA tested by DMM.
Please help point me out.
Thanks a lot!