Hello team,
My customer wants to synchronize the conversion timing of multiple ADS131M02.
Are below actions enough to accomplish synchronization of multiple devices? Is there anything else has to be done or missing settings to do synchronization?
1. Input negative pulse, which duration is longer than CLKIN but less than tw(RSL) into SYNC/RESET pin. Just like on the 8.5.2 of the datasheet.
2. Set the STATUS Register below F_RESYNC bit field #14 to 1b.
Best Regards,
Kei Kuwahara