Dear Expert
This is the schematic diagram before the change. We tested that applying surge interference would cause abnormal output of pin 11 .
The customer changed RSTSEL to add a pull-down 10K resistor, and RST to add a power down reset output low-level IC. Surge interference does not affect pin 11, and the output signal of pin 11 is normal.
May I ask why this phenomenon is caused by making such changes to the PIN16 and PIN22 pins controlled by the chip? I would like to consult FAE on how to configure pins 16 and 22.
Below is pcb layout :